News & Infos

Stability Perfected
Machines and systems always require stability. Heavy duty, large size element also emphasize the quality of the objects they support. Ganter has added…

Reliable and Corrosion-Resistant
Ganter continues to expand its selection of standard parts of A4 stainless steel – now including threaded plugs, magnetic plugs and robust oil sight…

Ganter e-Newsletter 10/2021
Side Clamps and Down-Thrust Clamps
Edge Protection Seal Profiles GN 2190
Application Video Clamping Knobs with Indexing Plunger

Ganter e-Newsletter 09/2021
Stainless Steel Latches GN 1150 in Hygienic Design
New Design for Pneumatically Operated Toggle Clamps
Upcoming Trade Shows

Perfect Latching
Wherever something needs to be adjusted, you will often find locking joints at work with serrations that define specific angle positions. To ensure…

Ganter e-Newsletter 08/2021
Stainless Steel Linear Guide Rail Systems
Couplings
Upcoming Trade Shows

Ganter e-Newsletter 07/2021
Quick Release Couplings GN 1050
Chemically Nickel Plated Power Clamps
Upcoming Trade Shows

A Connection That Won’t Let Go
To reduce the time involved in setting up equipment and production lines, Ganter has incorporated a new coupling in its product portfolio. With the GN…

Universally and Securely Fastened
Many things that hardly draw notice are nevertheless of elementary importance within the overall context. For example, it would be hard to conceive…