Elegantly designed and extremely functional: the new slam latches GN 936 from Ganter, secure against manipulation and available with or without…
Ganter was a winner of this years's iF Design Award, a world-renowned design prize. The cabinet "U" handles GN 422 won over the international jury,…
A sloped or uneven floor can be a challenge, such as when it is necessary to precisely align a machine. The new levelling feet GN 360 from Ganter…
Ganter is expanding its clamp mounting selection with new elements that will ensure simpler, more optimal and more flexible clamping of…
The jury of the German Design Award committee gave honor to our GN 126 flat adjustable tension levers, GN 328 and GN 428 cabinet "U" handles.
Elegantly covered or visibly bolted, available in a variety of surfaces and colors: The gripping trays GN 7330 and GN 7332 are new additions to the…
Invisible and highly mobile – exactly these requirements apply to the new GN 7237 Stainless Steel-Multiple-joint hinges, which are now included in the…
Ganter expands the product range of set collars. They can be used in multiple ways in machine and fixture fabrication.
Ganter is adding telescopic slides to its portfolio. With a wide range of extension types, additional functions and dimensions, these slides can…